-
Type:
Bug
-
Resolution: Fixed
-
Priority:
High
-
MCAL
-
MCAL-15390
-
-
MCUSW_J7_03.00.00
-
MCUSW_J7_10.00.00
-
j721e-evm
Hello,
Customer faced problem to use the whole memory space of the MT35XU512ABA1G12 NOR OSPI Flash device.
We figured out that driver was configured to use by default 3-bytes addressing mode.
After changing the configuration (by enabling the definition of "EXT_ADDRESS_ENABLE" on the code level) the erase operation still uses the 3 bytes addressing mode, as per its implementation:
Do we support 4 byte addressing in SDR mode ? if not why EXT_ADDRESS_ENABLE redundant macro is still being used.
E2E reference:
Regards
Tarun Mukesh