-
Type:
Bug
-
Resolution: Fixed
-
Priority:
Medium
-
Code Generation Tools
-
CODEGEN-11025
-
C2000_22.6.0.LTS
-
-
default
-
The only work around is to use --lfu_default=none and then explicitly mark all variables that need to be "preserved" using __attribute__((preserve)). This will avoid the default preserve behavior preserving the constant variables.
Bank0 App project ->
In .cmd: .const : > FLASH_BANK0_SEC3 , ALIGN(8) // address is 0x83000
In Bank0.map: (CORRECT)
.const 0 00083000 00000026
00083000 00000026 buck.obj (.const)
Bank1 App project ->
In .cmd: .const : > FLASH_BANK1_SEC3, ALIGN(8) // address is 0x93000
But still, in Bank1.map:
.TI.bound:$P$T19$2
* 0 00083000 00000026
00083000 0000000a buck.obj (.TI.bound:$P$T19$2)
0008300a 0000000a buck.obj (.TI.bound:$P$T20$3)
00083014 00000012 buck.obj (.TI.bound:$P$T18$1)
The compiler is "preserving" constant variables by default without requiring explicit "preserve" attribute. And when treating the constant variables as "preserve", the compiler is maintaining their addresses.
This is a problem because the Bank1 image is now writing not to Bank1 alone, but also Bank0. So it can lead to an issue of the same Bank being Erased/Programmed and Executed simultaneously, leading to unpredictable/incorrect behavior