HCI_EXT_SetTxPowerDbmCmd() does not change txPower on CC23XX device

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent
    • SimpleLink Lowpower SDK F3 BLE5 Stack
    • BLE_LOKI-754
    • BLE Stack BLE5-3.2.1 RC16
    • Hide
      BLE Stack BLE5-3.2.2
      BLE Stack BLE5-3.2.2 RC1
      Show
      BLE Stack BLE5-3.2.2 BLE Stack BLE5-3.2.2 RC1
    • CC2340R5

      SDK: 7.10

      Reproducibility: 100%

      The HCI_EXT_SetTxPowerDbmCmd() seems to not change the txPower of the device.

      A basic_ble project was used to reproduce this behavior.  A call to the HCI_EXT_SetTxPowerDbmCmd() function was added before the BLEAppUtil_initAdvSet() funciton call inside the Peripheral_start() function located in the app_peripheral.c file as shown below:

      status = BLEAppUtil_registerEventHandler(&peripheralAdvHandler);
      if(status != SUCCESS)
      {
          return(status);
      }
      
      // ADDITION START
      // 8dbm
      {
          const int8_t txPower = 8;
          const uint8_t fraction = 0;
          HCI_EXT_SetTxPowerDbmCmd(txPower, fraction);
      }    
      // ADDITION END
      status = BLEAppUtil_initAdvSet(&peripheralAdvHandle_1, &advSetInitParamsSet_1);
      if(status != SUCCESS)
      {
          // Return status value
          return(status);
      } 

       

      The value of the txPower variable was changed between -20dbm, 0dbm, and 8dbm. Regardless of the value used, there was no measurable difference in txPower. An RSSI measurement was conducted using a smart phone as a scanner and a current test was made using EnergyTrace (with display disabled, LED jumpers removed, and only 3.3V and GND pins connected between the LP-EM-CC2340R5 and the LP-XDS110ET) The results of these tests is shown below:

       

      Tx Power Measured RSSI Average Power Draw (30s)
      -20dbm -45 RSSI 0.1114mA
      0dbm -43 RSSI 0.1277mA
      8dbm -43 RSSI 0.1111mA

       
      These measurements show that there is no significant difference between the txPower settings.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4174 - HCI_EXT_SetTxPowerDbmCmd() does not...
                SYNCHRONIZED
                • Last Sync Date: