eDP to HDMI adaptors are failing

XMLWordPrintable

    • Type: Bug
    • Resolution: Duplicate
    • Priority: Medium
    • Processor SDK - Jacinto
    • ADASVISION-5955
    • PROCESSOR_SDK_09.00.00
    • PROCESSOR_SDK_10.00.00
    • Hide
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j721e-evm j721s2-evm j784s4-evm

      eDP to HDMI adaptors are failing.  No error is seen during init, but nothing is displayed on the screen when using it

      The ethfw is turned off as needed here, but the issue still remains across all SoC's.

      This could be a sysfw delta from 8.6 to 9.0, as this was working in 8.6

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            2 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4159 - eDP to HDMI adaptors are failing
                SYNCHRONIZED
                • Last Sync Date: