"Invalid CIO command (63)" error occurs when running application

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      The below error occurs when running an specific user program on an F280039C device:

      Invalid CIO command (63) in the CIO buffer at address (0xA000) was not recognized. Please check the device and program memory maps.

      0xA000 is writable memory.

      It appears to be some regression as there is no issue with CCS 12.1.0.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4136 - "Invalid CIO command (63)" error oc...
                SYNCHRONIZED
                • Last Sync Date: