enet: mdio: Failure in PHY reg read in manual mode in 'debug' profile

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Ethernet Switch Firmware
    • ETHFW-2242
    • ETHFW_09_00_00
    • ETHFW_10_00_00
    • j721e-evm

      PHY register read in manual mode appears to consistently fail in 'debug' profile image after migration to Clang v2.3.1.

      When the issue happens, Enet LLD is not able to ever recover.

      The error messages observed in the console are the following:

      Mdio_ioctlManualMode: failed to read PHY 0 C22 reg 0: -1
      EnetPhyMdioDflt_readC22: PHY 0: Failed to read C22 reg: -1
      EnetPhy_readReg: PHY 0: Failed to read reg 0: -1
      

      Note: Need to be confirmed that this issue is also reproducible in 'release' build.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4117 - enet: mdio: Failure in PHY reg read...
                SYNCHRONIZED
                • Last Sync Date: