[Safertos OSAL] Safertos configures MPU with MPU enabled which causes aborts

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent
    • PDK
    • PDK-13217
    • PROCESSOR_SDK_08.06.00
    • PROCESSOR_SDK_09.00.00
    • Hide
      j721e-evm
      j7200-evm
      j721s2-evm
      j784s4-evm
      j722s-hsfs-evm
      Show
      j721e-evm j7200-evm j721s2-evm j784s4-evm j722s-hsfs-evm

      Issue Description
      __mpu_init in OSAL SafeRTOS should disable the MPU before configuring it. If not, the MPU configuration can enter an invalid intermittent state.

      Resolution
      Disabled MPU before configuring MPU in the startup code.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4113 - [Safertos OSAL] Safertos configures...
                SYNCHRONIZED
                • Last Sync Date: