ECAP CSLR register definitions do not match TRM

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • PDK
    • PDK-12596
    • PROCESSOR_SDK_08.05.00
    • PROCESSOR_SDK_09.00.00
    • j721e-evm

      Issue Description:
      The register definitions in CSL does not match with the register definition in the TRM.

      For example:
      ECAP_PID is mentioned in TRM and CSL_ECAP_REVID is mentioned in CSL

      Also, 16-bit register write have been used to update some fields of the registers:

      It is not obvious that e.g. ECAP_ECINT_EN_FLG is the same as ECAP_ECEINT + ECAP_ECFLG."

      Resolution Description
      Fixed register names in CSL to use PID instead of REVID as a suffix.
       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4075 - ECAP CSLR register definitions do n...
                SYNCHRONIZED
                • Last Sync Date: