SBL Overrides IO Drive Strength Set by eFuse

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent
    • PDK
    • PDK-13030
    • PROCESSOR_SDK_08.06.00
    • PROCESSOR_SDK_09.00.00
    • Hide
      j721e-evm
      j721e-hsevm
      j721e-hsfs-evm
      Show
      j721e-evm j721e-hsevm j721e-hsfs-evm

      Issue Description:

      On J721E, SBL unconditionally overrides DRVSTRNGTH field in PADCONF registers in sbl_soc.c. Please refer to the below code:

      By writing 0xD, 0xD, 0xD … SBL overrides the die to die adjustments that may be done on ATE resulting in nom/fast/slow having the exact same behavior.

       

      static void J721E_SetupLvCmosDriveStrength(void)
      {
          volatile uint32_t *reg1 = (uint32_t *)0x43005008;
          volatile uint32_t *reg2 = (uint32_t *)0x4300500C;
          volatile uint32_t *lvcmos_drv_h_base = (uint32_t *)0x430060c0;
          volatile uint32_t *lvcmos_drv_v_base = (uint32_t *)0x430060d0;
          volatile uint32_t i;

          *reg1 = 0x68EF3490;
          *reg2 = 0xD172BC5A;

          /* Workaround for fixing lvcmos drive strength */
          for (i = 0; i < 4; i++)
          {        *(lvcmos_drv_h_base + i) = 0xD;        *(lvcmos_drv_v_base + i ) = 0xD;     }
      }

      Resolution Description:

      Drive strength field in PAD config register should be set as specified by efuse. Early silicon samples did not have full efuse programming, so SBL was programming 0xD as a workaround.
      Removed workaround from SBL

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4066 - SBL Overrides IO Drive Strength Set...
                SYNCHRONIZED
                • Last Sync Date: