Type casting issue in CDD IPC

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High

      Hello Team,

      In SDK ti-processor-sdk-rtos-j784s4-evm-08_06_00_14 Sciclient_rmIrqTranslateIrOutput was passed with wrong argument value because of type casting which is performed in file mcusw/mcal_drv/mcal/CddIpc/ipc_baremetal_hw/soc/V3/ipc_soc.c

      #define TISCI_DEV_COMPUTE_CLUSTER0_GIC500SS (uint8)58
      #define TISCI_DEV_MCU_R5FSS0_CORE0 (uint8)346
      #define TISCI_DEV_MCU_R5FSS0_CORE1 (uint8)347
      #define TISCI_DEV_R5FSS0_CORE0 (uint8)339
      #define TISCI_DEV_R5FSS0_CORE1 (uint8)340
      #define TISCI_DEV_R5FSS1_CORE0 (uint8)341
      #define TISCI_DEV_R5FSS1_CORE1 (uint8)342
      #define TISCI_DEV_R5FSS2_CORE0 (uint8)343
      #define TISCI_DEV_R5FSS2_CORE1 (uint8)344
      #define TISCI_DEV_COMPUTE_CLUSTER0_CLEC (uint8)44

      kindly request to correct this.

      E2E:https://e2e.ti.com/e2eprivate/bosch/bosch---ti-automotive-processors/f/bosch-dat3-jacinto-forum/1248729/tda4vh-cddipc-bug-in-sdk-08_06_00_14

      Thanks
      Tarun Mukesh

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-4065 - Type casting issue in CDD IPC
                ERROR
                • Last Sync Date: