CDD IPC communication with A72 for AEP/AHP

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • MCAL
    • MCAL-9613
    • MCUSW_J7_01.05.00
    • MCUSW_J7_09.00.00
    • Hide
      j7200-evm
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j7200-evm j721e-evm j721s2-evm j784s4-evm

      The CDD IPC driver configuration is missing the CDD_IPC_CORE_MPU1_0 option. This seems to have been previously supported but removed.

      Customers do need to use IPC between the AUTOSAR cores and the A72, and have been requesting this feature to be brought back.

      Support for A72 should be brought back in the CDD IPC driver and configuration.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3731 - CDD IPC communication with A72 for ...
                ERROR
                • Last Sync Date: