-
Type:
Bug
-
Resolution: Duplicate
-
Priority:
Not Prioritized
-
Code Generation Tools
-
CODEGEN-11194
-
-
default
-
For 3.0.0 STS and later versions of the compiler, the c7x::strm_eng and c7x::strm_agen C++ templates in c7x_scalable.h may be used for typedefs.
-
Behavior is as originally intended, so this is not a bug. Considering the issue as an enhancement, it is a duplicate of CODEGEN-9862.
The attached test case has these lines ...
/* ERROR */
__short32 vIn = __SE0ADV(__short32);
/* OK */
__short32 vIn2 = __SE0ADV(short32);
Build it ...
% cl7x file.cpp "file.cpp", line 9: error: identifier "__se_ac___short32" is undefined 1 error detected in the compilation of "file.cpp". >> Compilation failure
Similar problems are seen with the related macros __SE1ADV, __SE0, and __SE1.