[PSIRT-144] Accepts PairRandomSend before exchanging public key

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-4306
    • BLE Stack BLE5-2.2.7
    • Hide
      BLE Stack BLE5-2.2.8
      BLE Stack BLE5-2.2.8 RC12
      Show
      BLE Stack BLE5-2.2.8 BLE Stack BLE5-2.2.8 RC12
    • CC26X2R1

      The device responds with a PairRandomSend before PublicKeySend. Due to accepting PairRandomSend the implementation moves to a faulty state of the implementation where it is not able to complete pairing.

      The specification clearly shows the protocol flow in the standards but it does not explicitly state how to handle out-of-order protocol messages. Hence, this behavior can be attributed to under specification of the standards.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3806 - [PSIRT-144] Accepts PairRandomSend ...
                SYNCHRONIZED
                • Last Sync Date: