V4L2 driver compliance test is failing

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Linux Core SDK
    • LCPD-32334
    • 08.04.00
    • 10.01
    • Hide
      j721e-idk-gw
      j721e-sk
      j721s2-evm
      j721s2_evm-fs
      j784s4-evm
      Show
      j721e-idk-gw j721e-sk j721s2-evm j721s2_evm-fs j784s4-evm

      Running v4l2-compliance fails with 4 failures for imx390

      • may be the reason for v4l2-ctl's --stream-mmap not automatically finding resolution/format
      • v4l2-ctl --list-formats-ext -d18 spams "Size: Stepwise 8x1 - 16777216x16777216 with step 8/1" continuously{}

       

      Note:
      As an additional test, We used a USB camera which v4l2-ctl -d2 –stream-mmap works, but the v4l2-compliance still fails but with 1 failure.

      Manual page for v4l2-compliance: https://manpages.ubuntu.com/manpages/bionic/man1/v4l2-compliance.1.html

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3684 - V4L2 driver compliance test is failing
                SYNCHRONIZED
                • Last Sync Date: