[UART]: Driver does not support stop/timeout condition

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-12468
    • PROCESSOR_SDK_08.05.00
    • PROCESSOR_SDK_09.00.00
    • Hide
      j721e-evm
      j7200-evm
      j721s2-evm
      j784s4-evm
      Show
      j721e-evm j7200-evm j721s2-evm j784s4-evm

      Issue Description:

      UART protocol has a way to stop the RX data, as explained in the section 12.1.6.4.8.1.3.10 of the J7ES TRM. This is not implemented in the driver.

      Resolution Desciption

      Added interrupt handling for timeout. Added infra in driver to support the timeout interrupt handling.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3724 - [UART]: Driver does not support sto...
                SYNCHRONIZED
                • Last Sync Date: