[DOF]: Predictors are reset in the SET_PARAMS control command

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-12489
    • PROCESSOR_SDK_08.05.00
    • PROCESSOR_SDK_09.00.00
    • Hide
      j721e-evm
      j721s2-evm
      Show
      j721e-evm j721s2-evm

      DOF predictors are not reset in the SET_PARAMS ioctls. Because of which, if the predictors are changed in the same handle, dof does not work and returns error in the SubmitRequest API.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3725 - [DOF]: Predictors are reset in the ...
                SYNCHRONIZED
                • Last Sync Date: