[DSS/eDP]: Busy Waiting in eDP driver causes hang

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-12257
    • -
    • PROCESSOR_SDK_08.04.00
    • PROCESSOR_SDK_09.00.00
    • Hide
      j721e-evm
      j721s2-evm
      j784s4-evm
      Show
      j721e-evm j721s2-evm j784s4-evm

      Issue Description:

      Below code can cause hang in the display driver in case mailbox is empty. There should be timeout mechanism in this code to make sure driver exits gracefully and reports this error to the application.

       

      void messageReceive(DP_PrivateData *pD, DP_BusType busType)

      {

         :

                  /* read header first, to get size of message */

                  while (i < DP_MAILBOX_HEADER_SIZE)

                  {

                               mailboxEmpty = CPS_REG_READ(&regBase->mhdp_apb_regs.MAILBOX_EMPTY_ADDR_p);

       

                               /* test if mailbox is not empty */

                               if (0U == mailboxEmpty)

                              

      {                                      readVal = CPS_REG_READ(&regBase->mhdp_apb_regs.mailbox0_rd_data_p);                                      pD->rxBuffer[i] = (uint8_t)(readVal & 0x000000FFU);                                      *i++;*                          }

                  }

                  :

      }

      Resolution Description:

      Added check for busy waiting and break after a certain time period.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3722 - [DSS/eDP]: Busy Waiting in eDP driv...
                SYNCHRONIZED
                • Last Sync Date: