OFD utility -o option doesn't work if it is specified after the file name

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low

      The following command works as expected ...

      % ofd2000 --call_graph -o=stack_calls.xml file.out
      

      When the -o option is at the end of the command ...

      % ofd2000 --call_graph file.out -o=stack_calls.xml
      

      ... the output is not written to the file named with -o, but to stdout instead. It ends with ...

      error: failed to read "-o=stack_calls.xml"
      

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-3664 - OFD utility -o option doesn't work ...
                SYNCHRONIZED
                • Last Sync Date: