HE lost implicit conversions on vector with scalar operators

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Code Generation Tools
    • CODEGEN-10249
    • C7000_3.0.0.STS
    • C7000_3.1.0.LTS
    • default
    • Use an explicit cast on the scalar operand to the vector element type.

      Vector operators in which one operand is a scalar may not apply implicit conversions to the scalar operand in host emulation. For example, the following will result in a compilation error due to failing template argument deduction in host emulation:

      uint8_t op2;
      int16 foo(int * op1, int ch)

      { return ((int16)op1[ch]) * op2; }

      Workaround:
      If the scalar operand is explicitly cast to the element type of the vector, no compilation error will occur in host emulation:

      uint8_t op2;
      int16 foo(int * op1, int ch)

      { return ((int16)op1[ch]) * (int32_t) op2; }

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3473 - HE lost implicit conversions on vec...
                ERROR
                • Last Sync Date: