Linker help summary should not mention -h

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      When the linker is run from the command line with no arguments it begins ...

      % lnk2000
      TMS320C2000 Linker                      v22.6.0.LTS
      Copyright (c) 1996-2018 Texas Instruments Incorporated
      
      Usage: lnk2000 [-options] filename
      
      Use 'lnk2000 -h <option>' for more information on a particular option.  Use
      'lnk2000 -h <text>' to search options for information regarding <text>.
      

      That last paragraph about -h <option> is incorrect. The linker -h option says to make all global symbols static. When it is used to get more information about a particular option, confusing output is seen.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3655 - Linker help summary should not ment...
                SYNCHRONIZED
                • Last Sync Date: