Kingston 16G card could not boot to uboot prompt

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • Linux Core SDK
    • LCPD-17814
    • 2019.06
    • 09.01.00
    • j721e-idk-gw

      Among all the cards I have, this Kingston card could not boot to uboot prompt. Here is the log.

      Card info: Kingston 16G class10 UHS-1 microsd card.

      U-Boot SPL 2019.01-gbd3dc907f7 (Dec 16 2019 - 23:45:09 +0000)
      SYSFW ABI: 2.8 (firmware rev 0x0013 '19.10.0-v2019.10 (Terrific Llam')
      Trying to boot from MMC2
      Loading Environment from MMC... *** Warning - No MMC card found, using default environment
      
      Remoteproc 2 started successfully
      Starting ATF on ARM64 core...
      
      NOTICE:  BL31: v2.2(release):ti2019.04-447-ge516a38
      NOTICE:  BL31: Built : 02:53:49, Nov  1 2019
      I/TC: 
      I/TC: OP-TEE version: ti2019.04-190-g5208e5c-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Fri Nov  1 02:54:26 UTC 2019 aarch64
      I/TC: Initialized
      
      U-Boot SPL 2019.01-gbd3dc907f7 (Dec 16 2019 - 23:45:23 +0000)
      Detected: J7X-BASE-CPB rev E3
      Detected: J7X-VSC8514-ETH rev E2
      Trying to boot from MMC2
      ti_sci_power_domain_on: get_device(91) failed (-19)
      spl: mmc init failed with error: -110
      SPL: failed to boot from all boot devices
      ### ERROR ### Please RESET the board ###
      
      U-Boot SPL 2019.01-g350f3927b8 (Jan 03 2020 - 19:20:11 +0000)
      SYSFW ABI: 2.8 (firmware rev 0x0013 '19.10.1-v2019.10a (Terrific Lla')
      Trying to boot from MMC2
      Loading Environment from MMC... *** Warning - No MMC card found, using default environment
      
      Remoteproc 2 started successfully
      Starting ATF on ARM64 core...
      
      NOTICE:  BL31: v2.2(release):ti2019.04-447-ge516a38
      NOTICE:  BL31: Built : 02:53:49, Nov  1 2019
      I/TC: 
      I/TC: OP-TEE version: ti2019.04-190-g5208e5c-dev (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #1 Fri Nov  1 02:54:26 UTC 2019 aarch64
      I/TC: Initialized
      
      U-Boot SPL 2019.01-g350f3927b8 (Jan 03 2020 - 19:20:38 +0000)
      Detected: J7X-BASE-CPB rev E3                                                                                                                                          
      Detected: J7X-VSC8514-ETH rev E2
      Trying to boot from MMC2
      ti_sci_power_domain_on: get_device(91) failed (-19)
      spl: mmc init failed with error: -110
      SPL: failed to boot from all boot devices
      ### ERROR ### Please RESET the board ###
      
      

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3646 - Kingston 16G card could not boot to...
                SYNCHRONIZED
                • Last Sync Date: