-
Type:
Bug
-
Resolution: Fixed
-
Priority:
High
-
PDK
-
PDK-12213
-
PROCESSOR_SDK_08.00.00
-
PROCESSOR_SDK_10.00.00
-
Description
The RPMessage_getRemoteEndPtToken() function is used for looking up published end-points. If the function is invoked before any end-point is published, a taskWaiter element is used and added to a global queue that the RPMessage_ctrlMsgTask uses in the RPMessage_processAnnounceMsg() function to wake up the waiting thread.
The taskWaiter element is actually from the calling thread stack, and being added to a global queue using the stack variables as is. Customer is claiming that the pOsalPrms->lockHIsrGate(module.gateSwi) used to disable interrupts is not protecting against SVC instructions, and causing a stack corruption.
Resolution
Added a pool of 256 task waiter elements. During assignment a free one is assigned and added to queue. During free the task waiter element is identified by using proc id, service name and occupancy and same is removed from queue.