Assertion from EnetMcm_coreAttach API

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Ethernet Switch Firmware
    • ETHFW-2023
    • Hide
      ETHFW_08_01_00
      ETHFW_08_02_00
      ETHFW_08_04_00
      ETHFW_08_06_00
      Show
      ETHFW_08_01_00 ETHFW_08_02_00 ETHFW_08_04_00 ETHFW_08_06_00
    • ETHFW_09_00_00
    • Hide
      j721e-evm
      j7200-evm
      j784s4-evm
      Show
      j721e-evm j7200-evm j784s4-evm

      Since SDK 8.1 and 8.2, few customers have reported assertion due to EnetMcm_coreAttach() whereby the response being sent doesn't correspond to the command sent by MCM's client.

      One customer reported that the issue was the use of mailbox in MCM not being thread safe

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3579 - Assertion from EnetMcm_coreAttach API
                ERROR
                • Last Sync Date: