Cable connect/disconnect can cause CPSW unrecoverable condition

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Ethernet Switch Firmware
    • ETHFW-2084
    • Hide
      ETHFW_08_00_00
      ETHFW_08_01_00
      ETHFW_08_02_00
      ETHFW_08_04_00
      ETHFW_08_05_00
      ETHFW_08_06_00
      Show
      ETHFW_08_00_00 ETHFW_08_01_00 ETHFW_08_02_00 ETHFW_08_04_00 ETHFW_08_05_00 ETHFW_08_06_00
    • ETHFW_09_01_00
    • Hide
      j721e-evm
      j7200-evm
      j784s4-evm
      Show
      j721e-evm j7200-evm j784s4-evm

      Upon cable connection/disconnection of a MAC port with SGMII PHY, it's possible that CPSW can enter in an unrecoverable condition that requires device to be restarted.

      Typically, this issue causes RXBOTTOMOFFIFODROP statistics counter to increase for the corresponding MAC port.

      This issue is most likely to occur when cable connection/disconnection happens while there is active packet transfer of large frames.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            2 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3583 - Cable connect/disconnect can cause ...
                ERROR
                • Last Sync Date: