-
Type:
Bug
-
Resolution: Unresolved
-
Priority:
Medium
-
PDK
-
PDK-11973
-
PROCESSOR_SDK_08.02.00
-
PROCESSOR_SDK_10.01.00
-
Description:
The USART may erroneously clear or trigger the timeout interrupt when RHR/MSR/LSR registers are read.
Workaround:
For CPU use-case,
- If timeout interrupt is erroneously cleared
- OK since the pending data inside the FIFO will retrigger the timeout interrupt
- If timeout interrupt is erroneously set, and the FIFO is empty, use following SW workaround to clear the interrupt
- Set a high value of timeout counter in TIMEOUTH and TIMEOUTL registers
- Set EFR2 bit 6 to 1 to change timeout mode to periodic
- Read the IIR register to clear the interrupt
- Set EFR2 bit 6 back to 0 to change timeout mode back to the original mode
For DMA use-case,
- If timeout interrupt is erroneously cleared
- OK since the next periodic event will retrigger the timeout interrupt
- User must ensure that RX timeout behavior is in periodic mode by setting EFR2 bit 6 to 1
- If timeout interrupt is erroneously set
- This will cause DMA to be torn down by the SW driver
- OK since next incoming data will cause SW to setup DMA again