Variables tagged with section attributes not visible to debugger

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      Variables tagged with section attributes are not visible to debugger. Removing the attribute allows the debugger to 'see' the variable.

      When using the legacy symbol manager (via 'symbol_loader=1'). the variable is correctly resolved by CCS. However, I get the below error in the console:

      "Unable to read debug information (DWARF information is corrupted.); only the symbol table will be used."

      Hence the issue can be due to corrupt debug info.

      The out file was compiled with TI Clang v2.1.0

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            1 Vote for this issue
            Watchers:
            3 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3481 - Variables tagged with section attri...
                ERROR
                • Last Sync Date: