LTO: Compiling a source file with cortex-r4/r5 with -mthumb and linking with ARM mode cortex-r4/r5 runtime libraries improperly resolves an R_ARM_CALL relocation

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Generation Tools
    • CODEGEN-10000
    • ARMCLANG_2.1.0.LTS
    • ARMCLANG_2.1.1.LTS*
    • default
    • Hide
      This issue can be avoided if any of the following is true:
      - The compile and link steps of the build are performance as separate tiarmclang commands (as they are when building a project with Code Composer Studio (CCS))
      - Link-Time Optimization (LTO) is not enabled (-flto option is not used in compile and link tiarmclang command)
      - All C/C++ and assembly source files are compiled/assembled for ARM mode
      Show
      This issue can be avoided if any of the following is true: - The compile and link steps of the build are performance as separate tiarmclang commands (as they are when building a project with Code Composer Studio (CCS)) - Link-Time Optimization (LTO) is not enabled (-flto option is not used in compile and link tiarmclang command) - All C/C++ and assembly source files are compiled/assembled for ARM mode

      Compile and link a simple main() program containing a printf() call with -mthumb option:
      %> tiarmclang -mcpu=cortex-r4 -mthumb -mfloat-abi=soft -flto -O3 -v cutdown.c -o cutdown.out -Wl,-llnk.cmd,-mcutdown.map

      When the resulting cutdown.out is loaded and run with load470, the simulator fails to decode an instruction at the beginning of a runtime library function that was compiled in ARM mode.

      With Link-Time Optimization (LTO) turned on, the LTO generated object file contains a legitimate call from one ARM function to another ARM function that is annotated with a relocation to resolve the state and location of the callee function in the call instruction's opcode.

      Unfortunately, the handling of the relocation is changing the BL instruction into a BLX instruction that will put the processor in THUMB mode before it arrives at the start of the ARM mode callee function.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3408 - LTO: Compiling a source file with c...
                ERROR
                • Last Sync Date: