Incorrect source file chosen for function selected from modules view

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      To reproduce the issue I created the following folder structure:

      /

      + A/

      + namespace.h
      + namespace.cpp

      + B/

      + namespace.h
      + namespace.cpp

      + main.cpp

       

      The namespace.cpp files defines functions A::foo(int) and B::foo(int) as well as classes with functions A::C::bar(int) and B::C::bar(int).

       

      If I build and load the .out file in CCS with a projectless debug session, I can resolve the fully qualified names. More specific to this issue, I can go to the Modules view and click on the functions in the different namespaces and I am brought to the correct source files.

       

      To reproduce the bug, I first move the source files on my machine after building. Now CCS can’t use the paths in the .out file to find the exact files.

      Next I create a dummy CCS project and a debug configuration where I add the paths to A/ and B/ as source lookup paths. (You can also add the root folder containing both A/  and B/ instead.)

      Now when I click on A::foo or B::foo, I am brought to only one of the two namespace.cpp files. Which one I am brought to probably depends on search order.

      Since the source file lookup worked in the first case I described, this seems to be an issue in the way the IDE searches the source lookup paths.

       

       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3407 - Incorrect source file chosen for fu...
                SYNCHRONIZED
                • Last Sync Date: