XDS110: F28069 GPIO pins will unexpectedly switch state before erasing flash

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      When using an XDS110 debug probe, some F28069 GPIO pins will unexpectedly switch state for ~30us before erasing flash. This was observed my monitoring the GPIO pins in question.

      The below GPIO pins have been reported to exhibit the issue:

      GPIO 9
      GPIO 10
      GPIO 11
      GPIO 13
      GPIO 14
      GPIO 20
      GPIO 21
      GPIO 23
      GPIO 24
      GPIO 25

      This is not a comprehensive list. Other pins may also exhibit the issue but wasn't monitored.

      The issue apparently only happens with the XDS110. In both reported cases, there are no issues when swapping out the XDS110 with an XDS100 or XDS510

      The same issue also occurs when running the dbgjtag test via "Test Connection" button in the CCXML file.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            2 Vote for this issue
            Watchers:
            5 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3393 - XDS110: F28069 GPIO pins will unexp...
                SYNCHRONIZED
                • Last Sync Date: