OSAL: TimerP module restricts usage of up to max 4 DMTimer for R5Fs

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-11015
    • PROCESSOR_SDK_08.01.00
    • PROCESSOR_SDK_08.02.00
    • j721e-evm

      TIMERP_ANY_MASK for BUILD_MCU is defined as 0xF in osal/soc/j721e/osal_soc.h

      This restricts usage of up to max 4 DMTimer for R5Fs using TimerP APIs

      For J721E (with 10 MCU Domain DMTimers and 20 MAIN Domain DMTimers), there is no reason to restrict this to “4”.

      From osal/soc code review, it seems that the “TIMERP_ANY_MASK” definition in osal_soc.h for j721e is something which was copied from that for am65xx (AM65xx only had 4 MCU Domain DMTimers and 12 MAIN Domain DMTimers)

      __

      But for j721e we should restrict this to “8” (at least when running from MAIN Domain R5F cores) due to the following reason:-

      Interrupts for MAIN Domain DMTimer 0-11 are not directly connected MAIN R5Fs VIM
      There exists an Interrupt Router in between.

      Interrupts for MAIN Domain DMTimer 12-19 are directly connected MAIN R5Fs VIM
      Hence, the OSAL TimerP implementation is timerId=0 corresponds to MAIN Domain DMTimer 12 (timerId=1 -> MAIN Domain DMTimer 13 …..etc.. timerId=7 -> MAIN Domain DMTimer 19.)
      Note: This is same as SYSBIOS implementation.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3344 - OSAL: TimerP module restricts usage...
                SYNCHRONIZED
                • Last Sync Date: