UART instances 3-9 does not work on MAIN R5 in interrupt mode

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • PDK
    • PDK-11227
    • PROCESSOR_SDK_08.01.00
    • PROCESSOR_SDK_08.04.00
    • Hide
      j721e-evm
      j7200-evm
      j721s2-evm
      Show
      j721e-evm j7200-evm j721s2-evm

      UART instance 3-9 is are not working for MCU2_0 core in interrupt. Customer is using all the 10 instances on their board, instances 0-2 works fine but 3-9 does not work in interrupt mode. All the instances are working fine in polling mode. 

      On EVM, UART 4, connected to serial console, is also not working in interrupt mode for MCU2_0 but works fine in polling mode. 

      E2E link to the issue: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1078042/dra829v-uart-transmission-delay

       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3318 - UART instances 3-9 does not work on...
                SYNCHRONIZED
                • Last Sync Date: