GPIO_init clears external LF clock pin and stalls the device

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • TI Device Drivers
    • TIDRIVERS-5318
    • TIDRIVERS_6_10_00
    • TIDRIVERS_6_20_00
    • Hide
      CC13x1
      CC26x1
      CC13x2
      CC26x2
      CC13x2x7
      CC26x2x7
      CC13x4
      CC26x3
      CC26x4
      Show
      CC13x1 CC26x1 CC13x2 CC26x2 CC13x2x7 CC26x2x7 CC13x4 CC26x3 CC26x4

      If an external LF clock is configured in CCFG, the driverlib code will configure a mux in the selected DIO. Once you reach main(), GPIO_init's optimised startup routine will unconfigure all the pins, disabling the clock input and stalling the device.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3296 - GPIO_init clears external LF clock ...
                SYNCHRONIZED
                • Last Sync Date: