C2000 Flash - Custom GSxMSEL values are not checked correctly during restore sequence

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • Code Composer Studio Debugger
    • CCBT-3090
    • CCS_11.1.0
    • CCS_11.2.0
    • Generic

      Steps to reproduce:
      1. On F2837xD, set address 0x5F444 with value 0x67C0 on CPU1
      2. On CPU2, try to load a flash program.
      3. You will get a bunch of "Error setting the GSxMSEL register for Flash operations" errors

      This is because only the 0xF000 bits of the register are checked, but compared to the full value of the cache.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3278 - C2000 Flash - Custom GSxMSEL values...
                SYNCHRONIZED
                • Last Sync Date: