GapAdv_enable/disable sometimes creates null pointer access

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Urgent
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3716
    • BLE Stack BLE5-2.2.3
    • BLE Stack BLE5-2.2.4
    • Hide
      CC26X2R1
      CC2642R-Q1
      Show
      CC26X2R1 CC2642R-Q1

      Problem Description:

      The issue is triggered when there is a connection and application restarts the advertising after connection has established, then it might create null pointer access in multiple places in the software.

      Resolution:

      Added a NULL pointer check in the LL scheduler to check the return value with regards to secondary tasks, preventing the memory fault from occurring.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3264 - GapAdv_enable/disable sometimes cre...
                ERROR
                • Last Sync Date: