VISS mux output for R G and B planes hangs if additional outputs are not supplied

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low

      In order for R, G and B to be generated, the mux_output2, mux_output3 and mux_output4 all need to be set to 1.  Mux_output0 and mux_output1 are "don't cares" if you only need R, G and B and therefore the output images passed to these outputs can be NULL

      However, if these two values are set to 0 and the outputs are set to NULL, the VISS will hang.

      Additionally, this combination does not produce an output that looks to be correct when displaying the RGB using a display node.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-3250 - VISS mux output for R G and B plane...
                SYNCHRONIZED
                • Last Sync Date: