CUST SBL with SBL_SKIP_MCU_RESET should release MCU R5 before jumping to application

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • PDK
    • PDK-10536
    • PROCESSOR_SDK_08.00.00
    • PROCESSOR_SDK_08.01.00
    • j721e-evm

      In case of booting Linux from CUST SBL by skipping reset of MCU R5 then Linux is not able to attach to MCU R5 in IPC-only mode as the MCU1_0 is not released by the SBL.

      The SBL should call TISCI_MSG_PROC_RELEASE in the case where MCU reset is skipped (SBL_SKIP_MCU_RESET  is defined.

      A clean release from SBL will mean that A72 Linux can call TISCI_MSG_PROC_REQUEST and attach in IPC-only mode. This will enable IPC between MCU R5 and A72.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3232 - CUST SBL with SBL_SKIP_MCU_RESET sh...
                SYNCHRONIZED
                • Last Sync Date: