Update SysConfig to support Authentication pairing only feature and OOB pairing

XMLWordPrintable

    • Type: Enhancement
    • Resolution: Implemented
    • Priority: Medium
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3538
    • BLE Stack BLE5-2.2.3
    • BLE Stack BLE5-2.2.4
    • CC26X2R1

      A limitation of SysConfig prevents users from selecting both Authentication Only Pairing AND IO capabilities set to NoInputNoOutput.

      Those who enable OOB pairing are especially impacted by this limitation. Currently, Authentication Only Pairing must be disabled for those using OOB pairing (since IO capabilities must be set to NoInputNoOutput) . As a result, when non-CCC compliant phones send a pairing request before the peer device receives OOB data, then it will just resolve to just work pairing due to the IO capability being set to NoInputNoOutput.

      The above limitation was addressed and fixed.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3212 - Update SysConfig to support Authent...
                ERROR
                • Last Sync Date: