Resolving list does not overwrite LRU entry when GAPBOND_LRU_BOND_REPLACEMENT is enabled

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3617
    • Hide
      BLE stack BLE5-2.2.3 RC7
      BLE Stack BLE5-2.2.3
      Show
      BLE stack BLE5-2.2.3 RC7 BLE Stack BLE5-2.2.3
    • Hide
      BLE Stack BLE5-2.2.4 RC1
      BLE Stack BLE5-2.2.4
      Show
      BLE Stack BLE5-2.2.4 RC1 BLE Stack BLE5-2.2.4
    • CC26X2R1

      When the GAPBOND_LRU_BOND_REPLACEMENT in enabled and a new bond record is added after the bonding list is full and the resolving list has reached its limit, the resolving list does not overwrite LRU entry with the IRK of the new device.

      Fix:
      If the GAPBOND_LRU_BOND_REPLACEMENT is enabled and a new bond record is added to the resolving list using an existing bond index, then:

      Erase the current bond (form the NV and from the RL)
      Add a new bond record.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3207 - Resolving list does not overwrite L...
                ERROR
                • Last Sync Date: