[RTLS] Passive and connection monitor might fail to monitor one of the links when running 8 central responders topology

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3633
    • Hide
      BLE stack BLE5-2.2.3 RC5
      BLE Stack BLE5-2.2.3
      Show
      BLE stack BLE5-2.2.3 RC5 BLE Stack BLE5-2.2.3
    • BLE Stack BLE5-2.2.4
    • CC26X2R1

      [RTLS] Passive and connection monitor might fail to monitor one of links when running 8 central responders topology

      Root Cause:
      Collisions were observed when trying to monitor a new connection while the RF core is busy monitoring a different connection.

      Fix:
      Start monitoring new connection only if it's the first connection we are monitoring or if the RF is not busy.
      Otherwise, start monitoring the new connection when the current monitoring session ends.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3206 - [RTLS] Passive and connection monit...
                ERROR
                • Last Sync Date: