Long comment that does not begin with semicolon causes assembler to fail with: INTERNAL ERROR

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low

      The attached test case has this line ...

      ------------------------------------------------------sample_17-----------------------------------
      

      Build it ...

      % clpru file.asm
      "file.asm", INTERNAL ERROR!: Too many operands
      
      This may be a serious problem.  Please contact customer support with a
      description of the problem and a sample of the sourcefile that caused this
      message to appear.
      
      >> Compilation failure
      

      Add a semicolon to the start of that line, then it builds clean.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-3195 - Long comment that does not begin wi...
                SYNCHRONIZED
                • Last Sync Date: