Use of -save-temps causes warning diagnostic to not be emitted

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Low
    • Code Generation Tools
    • CODEGEN-9398
    • Hide
      C29_1.0.0.LTS
      ARMCLANG_5.0.0.STS
      ARMCLANG_4.0.0.LTS
      C29_2.0.0.STS
      ARMCLANG_2.1.3.LTS
      ARMCLANG_5.1.0.LTS
      ARMCLANG_3.2.2.LTS
      C29_2.1.0.STS
      C29_2.2.0.LTS
      Show
      C29_1.0.0.LTS ARMCLANG_5.0.0.STS ARMCLANG_4.0.0.LTS C29_2.0.0.STS ARMCLANG_2.1.3.LTS ARMCLANG_5.1.0.LTS ARMCLANG_3.2.2.LTS C29_2.1.0.STS C29_2.2.0.LTS
    • ARMCLANG_3.2.3.LTS*
    • default

      Please note that the -save-temps option is intended only for use in debugging an application when a developer would like to keep a compilation's intermediate file or representation that would normally be modeled as an internal data structure in the compiler.

      The compiler does not guarantee consistent diagnostic detection/reporting while using the -save-temps option.

      Original report:

      The attachment [^file.c]has these lines ...

          if (test < 10U);
          {
              func1(test);
          }

      Note the semi-colon on the first line.  While still legal C, it is probably a user error.

      Build it normally, and a warning diagnostic is emitted ...

      % tiarmclang -c file.c
      file.c:9:20: warning: if statement has empty body [-Wempty-body]
          if (test < 10U);
                         ^
      file.c:9:20: note: put the semicolon on a separate line to silence this warning
      1 warning generated.

      Add the option -save-temps and the diagnostic is not emitted ...

      % tiarmclang -c -save-temps file.c
      <nothing appears here>

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-3178 - Use of -save-temps causes warning d...
                SYNCHRONIZED
                • Last Sync Date: