SYS/BIOS cfg files do not open correctly with XGCONF editor in CCS 11

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium

      SYS/BIOS cfg files do not open correctly with XGCONF editor in CCS 11. The contents of the cfg file are blank. When clicking on some of the BIOS objects in the "Available Products" tab, the below error message occurs:

      An error has occurred. See error log for more details.
      Could not initialize class sun.awt.Win32FontManager

      There are no issues in CCS 10.4.0 when using the same version of SYS/BIOS and XDCTools.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            1 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3168 - SYS/BIOS cfg files do not open corr...
                SYNCHRONIZED
                • Last Sync Date: