-
Type:
Bug
-
Resolution: Unresolved
-
Priority:
Medium
-
Code Composer Studio
-
CCDSK-4126
-
-
-
Generic
As reported by user:
------
If I have several functions whose names differ only by namespace or class name, I can't select the one I want because the auto-completion doesn't show the fully-qualified names.
For instance, if I have two functions named "do_something" in two different namespaces or classes like this:
namespace1::do_something()
namespace2::do_something()
when I type "do_something" into the disassembly window search box I can't choose which one to go to.
One of the two will be chosen apparently at random.
There is no way to enter a fully-qualified name in this box and no way to select between multiple names with the same base name.
This can be reproduced on both CCS 10.4 and CCS 11.0.