[Mesh] LPN might fail to maintain friendship with ble.scanLatency < 10, when Display module is enabled

XMLWordPrintable

    • Type: Bug
    • Resolution: Unresolved
    • Priority: Medium
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3597
    • Hide
      BLE stack BLE5-2.2.3 RC6
      BLE Stack BLE5-2.2.4 RC5
      Show
      BLE stack BLE5-2.2.3 RC6 BLE Stack BLE5-2.2.4 RC5
    • BLE Stack BLE5-2.2.9
    • CC26X2R1

      When compiling an LPN node with ble.scanLatency < 10 (this is the default value, we've tested with 0), friendship terminates after LPN poll.

       

      note that the issue doesn't reproduce when using the same configuration without the display module.

       

       

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:

                Connection: Intermediate to External PROD System
                EXTSYNC-3133 - [Mesh] LPN might fail to maintain f...
                SYNCHRONIZED
                • Last Sync Date: