[Mesh][eRPC] (CC2652R7) Mesh LPN using eRPC is stuck after mesh init and static provisioning

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: High
    • SimpleLink CC13x2-26x2 SDK BLE5 Stack
    • BLE_AGAMA-3581
    • Hide
      BLE stack BLE5-2.2.3 RC5
      BLE Stack BLE5-2.2.3
      Show
      BLE stack BLE5-2.2.3 RC5 BLE Stack BLE5-2.2.3
    • BLE Stack BLE5-2.2.4
    • CC2652R7

      Problem Description

      CC2652R7 Mesh LPN using eRPC is stuck after mesh init and static provisioning

      The mesh is working with TBM

      The same is working on all other platforms

      The same working on CC2652R7 with other mesh roles

       Affected SDK Version: 5.30.00.55

      Steps to reproduce

      1. Flash CC2652R7 with LPN eRPC example
      2. Run mesh_init
      3. Try to run static provisioning

      Fix
      This issue was resolved after an update to the CoreSDK.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3128 - [Mesh][eRPC] (CC2652R7) Mesh LPN us...
                SYNCHRONIZED
                • Last Sync Date: