-
Type:
Bug
-
Resolution: Fixed
-
Priority:
High
-
SimpleLink CC13x2-26x2 SDK BLE5 Stack
-
BLE_AGAMA-3460
-
BLE Stack BLE5-2.2.2
-
-
Problem Description:
About ~200 bytes of heap is lost every connection established when the simple_mesh_node project is configured for in the "Mesh and Peripheral". This eventually leads to an assert that crashes the customer's application when heap space runs out.
SDK version tested: 5.20
Setup:
- In the simple_mesh_node project, change the Mesh Application to "Mesh and Peripheral".
- Add HEAPMGR_METRICS to track the heapmgrMemFreeTotal while debugging
- Record the heapmgrMemFreeTotal before entering a connection, then enter a connection with a smartphone.
- Disconnect from the device and you will see that heapmgrMemFreeTotal is ~200 bytes smaller than prior to connection establishment.
Alternate setup using Out of box firmware:
- Build and flash a default simple_mesh_node project.
- Initialize the node to advertise unprovisioned beacons.
- Using Lightblue, connect to the Simple mesh node and then disconnect, while recording the heapmgrMemFreeTotal. You should see the same behavior described above.
I have verified this on my end and observe ~200 bytes (200 bytes is not exact and varies for each connection/disconnection).