SYSCFG: Antenna switch within the SIP device package is defined as a board component

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • TI Device Drivers
    • TIDRIVERS-5072
    • TIDRIVERS_5_50_02
    • TIDRIVERS_5_70_00
    • Hide
      CC13x2
      CC26x2
      Show
      CC13x2 CC26x2

      Background

      The antenna switch for the SIP device is defined as a component in the board meta data, similar to the antenna switches for other boards (/launchpads) with this feature.

      Problem

      For the SIP package, the antenna switch is a component embedded in the device package, and is present regardless of board mount. That is, regardless of selection of "device" or "board" in SysConfig. In this case, the antenna switch is not a board component.

      Solution

      The antenna switch should be removed as a defined board meta data component, and any antenna switch logic will be handled internally by the RF module.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3088 - SYSCFG: Antenna switch within the S...
                SYNCHRONIZED
                • Last Sync Date: