Run out of UserKernelId when tivxAddKernelTIDL is called multiple times

XMLWordPrintable

    • Type: Bug
    • Resolution: Fixed
    • Priority: Medium
    • OpenVX Framework
    • TIOVX-1118
    • TIOVX_01.12.00
    • TIOVX_08.01.00
    • j721e-evm

      It looks like counter next_dynamic_user_kernel_id is incremented when new user kernel is allocated/added, but there is no way to decrement it.
      Because of this, when graph is created-removed multiple times, New User Kernel Id reaches to max limit and does not allocate new kernel id.

      It seems there is no way to decrement this counter, even if the vxRemoveKernel is called..

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3033 - Run out of UserKernelId when tivxAd...
                SYNCHRONIZED
                • Last Sync Date: