Uploaded image for project: 'Embedded Software & Tools'
  1. Embedded Software & Tools
  2. EXT_EP-10486

SBL booting u-boot and linux is failing for OSPI Boot

XMLWordPrintable

    • Icon: Bug Bug
    • Resolution: Won't Fix
    • Icon: Medium Medium
    • PDK
    • PDK-10389
    • Hide
      PROCESSOR_SDK_07.03.00
      PROCESSOR_SDK_08.00.00
      Show
      PROCESSOR_SDK_07.03.00 PROCESSOR_SDK_08.00.00
    • PROCESSOR_SDK_9.x
    • am65xx-evm
    • AM65xx is not supported by PDK anymore

      SBL fails to boot u-boot and linux in ospi mode. The u-boot throws error the following error: 

      NOTICE: BL31: v2.5(release):v2.5-83-g0693f35-dirty
      NOTICE: BL31: Built : 22:05:11, Jul 10 2021
      ERROR: GTC_CNTFID0 is 0! Assuming 200000000 Hz. Fix Bootloader
      U-Boot SPL 2021.01-g20e7036ac9 (Jul 10 2021 - 22:34:57 +0000)
      SYSFW ABI: 3.1 (firmware rev 0x0015 '21.5.0--v2021.05 (Terrific Llam')
      i2c_omap i2c@42120000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
      ti_i2c_eeprom_am6_parse_record: Ignoring record id 17
      Detected: Silicon SR1.0
      Detected: SER-PCIEUSBEVM rev E1
      SPL: Unsupported Boot Device!
      SPL: failed to boot from all boot devices

      ERROR ### Please RESET the board ###" 

       

            syncuser TI User
            syncuser TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved: