mcu1_0: Exception in NIMU example in SD card boot

XMLWordPrintable

    • Type: Bug
    • Resolution: Product No Longer Supported
    • Priority: Medium
    • Ethernet Switch Firmware
    • ETHFW-1843
    • ETHFW_08_00_00
    • j721e-evm
    • NDK is no longer supported. This issue is not observed with lwIP TCP/IP stack, hence rejecting.

      An abort is observed when running NIMU example application in SD card boot mode (SBL).

      This issue is related to Timer0 which NIMU adaptation layer gets upon requesting a timer to SYSBIOS using Timer_ANY flag.

      Timer0 is initially setup and used by SBL, but not cleanly freed before passing execution to MCU1_0 application - see PDK-8407.

            Assignee:
            TI User
            Reporter:
            TI User
            Votes:
            0 Vote for this issue
            Watchers:
            2 Start watching this issue

              Created:
              Updated:
              Resolved:

                Connection: Intermediate to External PROD System
                EXTSYNC-3002 - mcu1_0: Exception in NIMU example i...
                SYNCHRONIZED
                • Last Sync Date: